Full Chip simulator problem for MCF51JE256

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Full Chip simulator problem for MCF51JE256

1,440 Views
gustavod
Contributor III

Hi,

 

I'm using CodeWarrior 6.3 with MCF51JE256 microcontroller.

I'm able to compile my project, but when i try to do the full chip simulator there is no JE microcontroller into derivatives options.

 

Is there a workaround for that?

 

Best regards,

Gustavo

Labels (1)
Tags (1)
0 Kudos
Reply
2 Replies

1,285 Views
kef
Specialist I

Do you have JE256 service pack installed? CW 6.3. updates:

http://www.freescale.com/webapp/sps/site/overview.jsp?code=CW_UPDATES_MCU_63

0 Kudos
Reply

1,285 Views
gustavod
Contributor III

Yes. The service pack allows to compile the code, providing include files and libraries for JE256. Without this service pack is impossible to compile code for JE256/128.

 

However, apparently full chip simulator is not supported.

0 Kudos
Reply