FlexBus Processor Expert Bug?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FlexBus Processor Expert Bug?

2,164 Views
kackle123
Contributor IV

When using Processor Expert (PE) in a MK64FN1M0VLQ12 bare metal project within CodeWarrior 10.6, the FlexBus component/bean (Init_FB) doesn't allow me to point its Memory block 0 to 0x60000000.  It responds with the error "There is no access into memory from 0x60000000 to 0x60000001".  Is this a bug?

0 Kudos
Reply
4 Replies

1,963 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Joe,

This is not a  bug . The Flexbus address allowed range is 0x6000 0000 - 0xDFFF FFFF .

Processor Expert reminder it , also the Reference Manual of chip MK64FN1M0VLQ12 show it :

pastedImage_2.png

pastedImage_1.png

Hope it helps,


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,963 Views
kackle123
Contributor IV

But I am not trying to enter a base address of 0x50000000; I am trying to enter 0x60000000.

0 Kudos
Reply

1,963 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hi Joe,

Please share your project .

BR

Alice

0 Kudos
Reply

1,963 Views
kackle123
Contributor IV

I included a picture of the FlexBus (Init_FB) Processor Expert (PE) component:

PE_FlexBus.gif

To recreate the problem:

1) Create a new MK64FN1M0VLQ12 (LQFP 144-pin package) project with PE within CodeWarrior 10.6.

2) Add component Init_FB to its PE.

3) Populate the Init_FB's values in the same way shown in the picture above.

No start address that you enter is allowed.

0 Kudos
Reply