FMPLL configuration for MPC5644A

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FMPLL configuration for MPC5644A

1,700 Views
chandrasekarkri
Contributor III

pls help anyone how to configure fmpll in mpc5644a by Fref =40 MHZ for Fsys=120MHZ
i configured but it not working in EVT board ..my configuration is
void FMPLL_config()
{
ECSM.MUDCR.R = 0x40000000; /* 1 SRAM waitstate for fsys above 98MHz */
FMPLL.ESYNCR2.R = 0x00000002;
FMPLL.ESYNCR1.R = 0xF0020024;
while (FMPLL.SYNSR.B.LOCK != 1) {}; /* Wait for FMPLL to LOCK */
FMPLL.ESYNCR2.R = 0x00000001; /* Fsys =120Mhz */
SIU.ECCR.R = 0x00001003; /* CLKOUT to /4 because of 66MHz limit */

}

Labels (1)
2 Replies

1,553 Views
martin_kovar
NXP Employee
NXP Employee

Hi,

try this configuration:

/* Set sysclk = 120MHz running from PLL with 40 MHz crystal reference. */

void initSysclk (void) {

      FMPLL.ESYNCR1.B.CLKCFG = 0X7;       /* Change clk to PLL normal mode from crystal */

      FMPLL.SYNCR.R = 0x22880000;                  /* Fsys =60Mhz */

      while (FMPLL.SYNSR.B.LOCK != 1) {}; /* Wait for FMPLL to LOCK  */

      FMPLL.SYNCR.R = 0x22800000;                  /* Fsys =120Mhz */

}

Regards,

Martin

1,553 Views
chandrasekarkri
Contributor III

Hi Martin Kovar,

I tested your code in my XPC564A 324BGA MINIMODULE BOARD(MPC5644A), but board is not responding..do you have any suggestions for this..

Regards,

Chandrasekar K

0 Kudos
Reply