Download process for 908QT4 demo board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Download process for 908QT4 demo board

Jump to solution
2,540 Views
FransW
Contributor I
I wish to use Codewarrior which was purchased with a MC68HC908QT4 demo board. Unfortunately I can find no specific info on how to use the system. Lots of general help but nothing specific to the use of this board.

I can intialise the project manager when I start a new project for an assembler application, specifying the above processor and the fact that I want to use an absoulte assembler program. The main window remains grey and all the icons except the file icons remain grey. I assume that I would need to do something to make the main window active? When I try to 'make' one of the absolute assembler demo projects, it says that no CPU is defined but how do I do this? Once this is done, how would I download the code to the demo board?

Am I missing some documentation or is there some electronic source that will give me some idea on how to use this system?

Thanks for your help
Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
704 Views
CrasyCat
Specialist III

Hello

I assume you are using CodeWarrior for HC08 V5.0. Am I right?

Take a look at the attached technical note.
It explains how to create an absolute assembly project with CodeWarrior HC08 V5.0.

CrasyCat

 

TN245.pdf

Message Edited by t.dowe on 2009-09-16 10:43 AM

View solution in original post

0 Kudos
Reply
1 Reply
705 Views
CrasyCat
Specialist III

Hello

I assume you are using CodeWarrior for HC08 V5.0. Am I right?

Take a look at the attached technical note.
It explains how to create an absolute assembly project with CodeWarrior HC08 V5.0.

CrasyCat

 

TN245.pdf

Message Edited by t.dowe on 2009-09-16 10:43 AM
0 Kudos
Reply