Current tutorials/books/reference materials.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Current tutorials/books/reference materials.

Jump to solution
4,226 Views
jamesepps
Contributor I

I have a project that was dropped onto me. I have C experience but am just now learning C for MCUs. Have a K60 based engine controller built and ready to code. Was given the project with Codewarrior 10.6 partially configured, and I can do simple things like pull I/Os high to start an engine but nothing else. Nothing else other than a few I/Os and our LCD id configured to initialize though. I new to CodeWarrior and need links to required tutorials, or full books I can buy on CodeWarrior configuration specifically Processor Expert to start. I am only halfway understanding everything so far :-(

Labels (1)
0 Kudos
Reply
1 Solution
3,862 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

HI

First i suggest you refer below courses for CW10 studying

CodeWarrior for Microcontrollers-Eclipse IDE|Freescale

here is some useful manuals

CodeWarrior for Microcontrollers-Eclipse IDE|Freescale

we can also find some useful manuals under CW install folder

C:\Freescale\CW MCU v10.6.4\MCU\Help\PDF

and demo code:

C:\Freescale\CW MCU v10.6.4\MCU\CodeWarrior_Examples\Kinetis_Examples

processor expert demo code:

C:\Freescale\CW MCU v10.6.4\MCU\CodeWarrior_Examples\Processor_Expert\Kinetis

Hope this helps!


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

4 Replies
3,862 Views
BlackNight
NXP Employee
NXP Employee

Hi James,

in addition to the references to the previous reply, here is a tutorial you might use:

There are other tutorials on this site which are applicable for your board too.

I hope this helps,

Erich

0 Kudos
Reply
3,863 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

HI

First i suggest you refer below courses for CW10 studying

CodeWarrior for Microcontrollers-Eclipse IDE|Freescale

here is some useful manuals

CodeWarrior for Microcontrollers-Eclipse IDE|Freescale

we can also find some useful manuals under CW install folder

C:\Freescale\CW MCU v10.6.4\MCU\Help\PDF

and demo code:

C:\Freescale\CW MCU v10.6.4\MCU\CodeWarrior_Examples\Kinetis_Examples

processor expert demo code:

C:\Freescale\CW MCU v10.6.4\MCU\CodeWarrior_Examples\Processor_Expert\Kinetis

Hope this helps!


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

3,862 Views
jamesepps
Contributor I

One more question. There is a Kinetis K60 Tower included with all the hardware. any documentation on that TWR-K60N512 model

0 Kudos
Reply
3,862 Views
jamesepps
Contributor I

Sorry to waste your time with the tower. I found the information I needed.

0 Kudos
Reply