Content of a .CRT file

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Content of a .CRT file

879件の閲覧回数
FabioPdM
Contributor I

Hi, 

I have some static bytes in the source file like a stamp.

When I search for this stamp in the .crt file that will be loaded in the MC it does not exist.

Any one could help me?

0 件の賞賛
返信
4 返答(返信)

832件の閲覧回数
FabioPdM
Contributor I

Hi Alice,

    In time, I forgot to mention that this .CRT file have 0x0D 0x0A record separators.

    Could be that this file a Freescale SRecord format?

    If so I can create it again with CW easily!!!

0 件の賞賛
返信

844件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @FabioPdM 

For better help you, please tell us the part number of your MCU, thanks.

 

 

BR

Alice

0 件の賞賛
返信

834件の閲覧回数
FabioPdM
Contributor I

Hi Alice,

      The target is MCU MC9S08AW32 and to burn it  they use a .CRT file extension that I dont know how it is created and file format.

       That's the reason that I am investigating how this file extension was created to solve the doubt.

       This file extension .CRT give any clue how can I generate it in the CW?

       The first 16 bytes in the .CRT file are ( hex 0x ) 61 69 73 64 7F 7D 43 5A 43 5D 5D 5F 44 47 5B 5E 6F 5E 73 42 ( 'aisd' )    .

       Thanks for your help!!!

0 件の賞賛
返信

806件の閲覧回数
Itzzamna_Supp
NXP TechSupport
NXP TechSupport
When compiling, S19 is generated and remains in the FLASH folder, the SRecord file type is saved there in S19, where you will find the CRT.
0 件の賞賛
返信