Compiler Error " Illegal storage class" in Header file

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Compiler Error " Illegal storage class" in Header file

ソリューションへジャンプ
13,421件の閲覧回数
Hombre
Contributor I

CodeWarrior IDE Version 4.2.6.895

HCS12A256

 

Hi all,

 

i have a little problem with the Compiler. I am on a project to create a Bootloader running in RAM for reprogramming flash memory. The -Pic –PicRTS options are activated for position independent code.

The Problem is that I receive the Compiler Error “Illegal storage class” for this definition in a Header File:

 

typedef struct

{

 unsigned char data[0x800];

 …..

 …..     

} STR_FPGA_MEM;

 

 

I can’t see the problem. Could somebody help me?

 


Thanks

Daniel

 

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
4,838件の閲覧回数
CompilerGuru
NXP Employee
NXP Employee
Hi Daniel,

the code snippet you copied looks OK, so I could imagine two causes
- either it is in the parts you did cut away. For example a not correctly terminated declaration before the copied snippet
- or, and I guess that's the most likely explanation, you have some sort of name collision with a macro.
  could be data or STR_FPGA_MEM.
  Such problems are best seen with the preprocessor output, use the context menu in the project view.
  I could bet it a macro :smileyhappy:

Daniel

元の投稿で解決策を見る

0 件の賞賛
返信
8 返答(返信)
4,838件の閲覧回数
bob_walker
Contributor III

I, too, have gotten bitten by this one. One would think that if the parsed line is unterminated by a semicolon, and the end of file is reached, an error for the offending line should be generated.

 

Who in their right mind would continue a C statement ACROSS files?!

0 件の賞賛
返信
4,838件の閲覧回数
CompilerGuru
NXP Employee
NXP Employee

Well, it's legal in ANSI C.

And there may be some uses for it when including the same file multiple times with different defines.

I agree that normally you would not do this for a statement, but for example it could make sense to do it for initialization data.

 

You can propose this as feature request using the support system to at least issue a warning when a statement crosses multiple files.

 

Daniel

0 件の賞賛
返信
4,839件の閲覧回数
CompilerGuru
NXP Employee
NXP Employee
Hi Daniel,

the code snippet you copied looks OK, so I could imagine two causes
- either it is in the parts you did cut away. For example a not correctly terminated declaration before the copied snippet
- or, and I guess that's the most likely explanation, you have some sort of name collision with a macro.
  could be data or STR_FPGA_MEM.
  Such problems are best seen with the preprocessor output, use the context menu in the project view.
  I could bet it a macro :smileyhappy:

Daniel
0 件の賞賛
返信
4,838件の閲覧回数
PaoloSubiaco
Contributor I
Hi add this post just for reference for those who see the same compile error:
in my case, I forgot the semicolon after a declaration in one include file:

// File rtc.h
// ........
// Function prototypes
void oneFunction(void);
unsigned char secondFunction(void);
void thirdFunction(void)

//End of rtc.h : Look at the last function, not terminated by semicolon!!!


I spent about two hours to discover this error.... Codewarrior compiler should be improved, though.
Best regards. Paolo
0 件の賞賛
返信
4,838件の閲覧回数
Lundin
Senior Contributor IV

Didn't you rather get two errors? First "illegal storage class" and then "missing semicolon".

 

Also, if you haven't gotten burned by strange missing semicolon errors over and over yet, don't worry. This is an initation rite all C programmers have to go through during their first 5 years or so, until they eventually learn to type out semicolons in their sleep. :smileyhappy:

 

0 件の賞賛
返信
4,838件の閲覧回数
irob
Contributor V

Truer words, never spoken, Lundin.

0 件の賞賛
返信
4,838件の閲覧回数
irob
Contributor V

Wow, this got me too!  Even with the hint of it being a prototype declaration, it still took me a while to find.

0 件の賞賛
返信
4,838件の閲覧回数
Hombre
Contributor I
Hi,
 
thanks for help Daniel. Finally i found the macro :smileyhappy:
 
Best regards
Daniel
0 件の賞賛
返信