Command Window 3.1 History limitation?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Command Window 3.1 History limitation?

Jump to solution
3,502 Views
hwrobel
NXP Employee
NXP Employee
It seems that the command history of the TCL Command Window 3.1 in CW for EPPC fills up to 250 entries and then simply stops, i.e., it neither drops the oldest entries, nor does it enlarge the history.

Does anyone know of a way to turn the history into a circular buffer, or clear it, or increase the max entry count?

Thanks!
Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,882 Views
marc_paquette
Contributor V

The command history is indeed circular. Unfortunately, the IDE doesn't adjust the command history numbers, preventing you from using the "! number" command repeat syntax in any useful way.

I've forwarded your comment along to the IDE team. I can also suggest that you submit a bug report if you'd like to keep track of this situation.

To submit a service request:

1. Go to http://freescale.com/support

2. In the Develop column, click "Technical Support."

3. Click "Submit a service request."

Marc.

View solution in original post

0 Kudos
Reply
1 Reply
1,883 Views
marc_paquette
Contributor V

The command history is indeed circular. Unfortunately, the IDE doesn't adjust the command history numbers, preventing you from using the "! number" command repeat syntax in any useful way.

I've forwarded your comment along to the IDE team. I can also suggest that you submit a bug report if you'd like to keep track of this situation.

To submit a service request:

1. Go to http://freescale.com/support

2. In the Develop column, click "Technical Support."

3. Click "Submit a service request."

Marc.

0 Kudos
Reply