Command Line on-board flash programmer for 9S12

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Command Line on-board flash programmer for 9S12

ソリューションへジャンプ
3,698件の閲覧回数
darrin
Contributor II
Hello,
 
I am using CodeWarrior 4.5 for the 9S12 and the P&E USB multilink programmer.
I can program the on-board flash by clicking "debug" in the IDE which calls hiwave debugger.
Is there a command-line way to program the on-board 9S12 flash?
 
Thanks
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,808件の閲覧回数
CrasyCat
Specialist III
Hello
 
We do not have command line tools to do production flash programming.
If you are looking for production flash programming tool you can check with P&E (www.pemicro.com).
 
They have production flash programming tools for HCS12.
 
CrasyCat

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,809件の閲覧回数
CrasyCat
Specialist III
Hello
 
We do not have command line tools to do production flash programming.
If you are looking for production flash programming tool you can check with P&E (www.pemicro.com).
 
They have production flash programming tools for HCS12.
 
CrasyCat
0 件の賞賛
返信