Codewarrior project for MCF52259

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Codewarrior project for MCF52259

1,315 Views
henryzhang62
Contributor I

I have a Codewarrior project for MCF52259.

After importing it with CW11, run/debug configuration does not have  link to P&M multilink USB JTAG

and no MCU selection for MCF52259 during importing from General Project.

Is anything missing for my importing?

Thanks.

---henry

0 Kudos
Reply
1 Reply

1,213 Views
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Henry,

In which CodeWarrior version was your project originally created? Also, make sure that you have the ColdFire processors installed in CodeWarrior 11.

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 Kudos
Reply