Codewarrior DSC linker map file

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Codewarrior DSC linker map file

2,178 Views
Lucas42
Contributor I

Hi,

I'm working on an old project with Codewarrior 8.3 and DSC 56F8347.

In the linker cmd file (used by Codewarrior) the RAM section is the following:

.ApplicationData :
{
# save space for the pROM data copy
. = ALIGN(2);

. = __xRAM_data_start + __data_size;

# .bss sections
* (rtlib.bss.lo)
* (rtlib.bss)
. = ALIGN(4);
F_Xbss_start_addr = .;
_START_BSS = .;
* (.bss.char) # used if "Emit Separate Char Data Section" enabled
* (.bss)
_END_BSS = .;
F_Xbss_length = _END_BSS - _START_BSS;

/* Setup the HEAP address */
. = ALIGN(4);
_HEAP_ADDR = .;
_HEAP_SIZE = 0x00000100;
_HEAP_END = _HEAP_ADDR + _HEAP_SIZE;
. = _HEAP_END;

/* SETUP the STACK address */
_min_stack_size = 0x00000500;
_stack_addr = _HEAP_END;
_stack_end = _stack_addr + _min_stack_size;
. = _stack_end;

/* EXPORT HEAP and STACK runtime to libraries */
F_heap_addr = _HEAP_ADDR;
F_heap_end = _HEAP_END;
F_Lstack_addr = _HEAP_END;
F_StackAddr = _HEAP_END;
F_StackEndAddr = _stack_end - 1;

# runtime code __init_sections uses these globals:

F_Ldata_size = __data_size;
F_Ldata_RAM_addr = __xRAM_data_start;
F_Ldata_ROM_addr = __pROM_data_start;

F_xROM_to_xRAM = 0x0000;
F_pROM_to_xRAM = 0x0001;

F_start_bss = _START_BSS;
F_end_bss = _END_BSS;

__DATA_END=.;

} > .x_Data

In the xmap file, I have following segments addressed:

BSS address start0x00000104
BSS length0x00000511
BSS address end0x00000615
HEAD address start0x00000618
HEAP length0x00000100
HEAP address end0x00000718
STACK address start0x00000718
STACK address length0x00000500
STACK address end0x00000C18

Furthermore, I have in the xmap BSS section all variable listed in address order with own size.

Tha main problem is that some of this variables haves an address that is outside the BSS section even if they are in the BSS section and on the left of this variable, near the address, a "B" is listed (follow an example)

   000003A7 00000001 .bss    FsTxStato	(sci.c)
   000003A8 00000001 .bss    FsRxStato	(sci.c)
B  00000750 00000001 .bss    FgFasiTestCLAMP2	(T0_Test.c)
B  00000751 00000001 .bss    FgFasiTestCLAMP1	(T0_Test.c)
B  00000752 00000001 .bss    FgCLAMP2InTest	(T0_Test.c)
B  00000753 00000001 .bss    FgCLAMP1InTest	(T0_Test.c)
   000003AA 00000001 .bss    FSR_lock	(Cpu.c)
   000003AB 00000001 .bss    FSR_reg	(Cpu.c)

The second problem is that some variable in the BSS section haves the address inside the BSS section but are out of order and searching for their address seems to be overlapped with other variable. Also those variables haves a "B" on the left side. (follows an example with the variable at address 0x00000223)

   00000111 00000001 .bss    FsStatoAd	(AD.c)
B  00000223 00000001 .bss    FgOutFlg	(AD.c)
   00000112 00000001 .bss    FsTastoStopOld	(Alarm_Manager.c)
...
...
...
   00000216 00000054 .bss    FgDpTimer100ms	(EM_01_Scheduler.c)
   0000026A 0000001E .bss    FgDpTimer5ms	(EM_01_Scheduler.c)
   00000288 000000D2 .bss    FgDpTimer1ms	(EM_01_Scheduler.c)

I have searched for xmap documention but didn't find anything.

Someone can give me a tip? What is the "B" on the left side of this variables?

Thanks

.

0 Kudos
Reply
2 Replies

2,168 Views
Lucas42
Contributor I

Does anyone have any information on the meaning of that "B"?

Or any information/documentation on xmap file format?

Thanks.

0 Kudos
Reply

2,108 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Pls refer the description in the screenshot:

xiangjun_rong_0-1659609254521.png

I attach the doc Targeting_56800E_cd.pdf

Hope it can help you

BR

XiangJun Rong

 

0 Kudos
Reply