Codewarrior 10.6 issues with MKE02

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Codewarrior 10.6 issues with MKE02

1,327件の閲覧回数
juancazares
Contributor I

I am using a kinetis MKE02Z64 microcontroller with Codewarrior 10.6, I read in the datasheet that this micro has up to 57 GPIOs divided in portA, B, C, D, E, G, H. however after I created a bareboard project i can see only defines for portA and portB. What is wrong?

ラベル(1)
0 件の賞賛
返信
1 返信

1,138件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Juan,

For each GPIO1 register is 32 bit ,

The PORTA0-32(module signal name) include PTA(PTA0-7, total 8 pins) PTB PTC PTD (chihp signal name) ,

please check this table on the ke02 reference manual :

pastedImage_0.png

If still have question ,please contact us without any hesitate .


Have a great day,
Alice Yang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信