Codewarrior 10.2 programs flash in Kinetis 100x slower than MCU 10.1.  Using J-link

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Codewarrior 10.2 programs flash in Kinetis 100x slower than MCU 10.1.  Using J-link

ソリューションへジャンプ
1,865件の閲覧回数
deuteron
Contributor II

We just upgraded from MCU 10.1 to MCU 10.2. We run and debug programs in a Kinetis K10 out of internal flash. We use a J-link version 8.0 or a Kwik-stik for download. Programming the flash takes about 2 seconds with 10.1 but over 3 minutes with version 10.2. This has been tried on different computers, all use Windows 7. Are we doing something wrong? Is this a know issue? Need some suggestions

ラベル(1)
0 件の賞賛
返信
1 解決策
1,233件の閲覧回数
deuteron
Contributor II

With CW-MCU 10.1, the defauslt J-Link setting is "Auto" but the default for CW 10.2 is "fixed". To change the speed:

 

Main menu -> Run -> Debug Configurations -> Main -> Connection -> Edit -> JTAG/SWD speed -> Auto.

 

Then it loads at the proper speed.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,234件の閲覧回数
deuteron
Contributor II

With CW-MCU 10.1, the defauslt J-Link setting is "Auto" but the default for CW 10.2 is "fixed". To change the speed:

 

Main menu -> Run -> Debug Configurations -> Main -> Connection -> Edit -> JTAG/SWD speed -> Auto.

 

Then it loads at the proper speed.

0 件の賞賛
返信