CodeWarrior for MCU 7.2 + Debug + writeaddressreg error. writecontrol 6145 0x200000000 failed.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CodeWarrior for MCU 7.2 + Debug + writeaddressreg error. writecontrol 6145 0x200000000 failed.

ソリューションへジャンプ
5,172件の閲覧回数
ssinfod
Contributor IV

Hello,

 

I have CodeWarrior 7.2 for MCU running inside a WindowsXP VirtualMachine (virtualbox).

I'm trying to start a Debug session on a M52233DEMO board which has its own BDM on the demo board.

 

Right now, when I start the Debug session I have the following error (see attached image):

writeaddressreg error. writecontrol 6145 0x20000000 failed.

 

Does anybody know what could cause this error / message ?

 

Thanks

ssinfod

ラベル(1)
1 解決策
4,781件の閲覧回数
ssinfod
Contributor IV

I found the solution while going over the project Settings !

Indeed, my project properties for the "CF Debugger Settings" were for the wrong MCU target. (5208 vs 52233).

Once I changed it from the from the project Settings (ALT+F7), then the Debug session was working perfectly !

See attached image for screenshot.

Sorry for the noise... maybe it will help somebody.

ssinfod

元の投稿で解決策を見る

1 返信
4,782件の閲覧回数
ssinfod
Contributor IV

I found the solution while going over the project Settings !

Indeed, my project properties for the "CF Debugger Settings" were for the wrong MCU target. (5208 vs 52233).

Once I changed it from the from the project Settings (ALT+F7), then the Debug session was working perfectly !

See attached image for screenshot.

Sorry for the noise... maybe it will help somebody.

ssinfod