CodeWarrior for HCS12 uP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CodeWarrior for HCS12 uP

4,552 Views
jes
Contributor I
Hi,
 
I recently downloaded an evaluation version of CodeWarrior for the HCS12 family.  I was intending to use it for the MC9S12E256 uP.  However, this uP is not listed as one of the 'derivatives' during initial project creation.  Is this processor indeed supported?
 
Also, I've used CodeWarrior IDE and debugger for an HCS08 processor.  Are there any major distinctions between the two IDEs or debugger or other capabilities that I should keep in mind?
 
Thanks.
 
JES
Labels (1)
Tags (1)
0 Kudos
Reply
5 Replies

2,602 Views
quebec
Contributor I
Hi,
 
Could you please help me? I could find an evaluation version for HC12, but could not find the same SW for HCS12.
 
Could you please provide me with the URL?
 
Thanks.
 
Best Regards.
0 Kudos
Reply

2,602 Views
Alban
Senior Contributor II
Hello Quebec,
 
This is the same.
CodeWarrior v4.5 also covers S12 and S12X.
 
Cheers,
Alban.
 
Please refrain from crossposting not to divide work and mutliply identical answers.
Crossposts are deleted.
0 Kudos
Reply

2,602 Views
quebec
Contributor I
Thanks Alban,
 
Sorry for my CrossPost.
 
I have downloaded the 4.6 version and come back to you if any problem.
 
Thanks again.
 
Best Regards,
 
Stéphane
0 Kudos
Reply

2,602 Views
Alban
Senior Contributor II
Hi Stéphane,
 
I didn't even know there was a 4.6 for S12(X) now !
That's me downloading the +300MB ...
 
Cheers,
Alban.
0 Kudos
Reply

2,602 Views
CrasyCat
Specialist III
Hello
 
Which version of CodeWarrior for HCS12 are you using?
To retrieve that information go to Help -> About Metrowerks CodeWarrior or help -> About Freescale CodeWarrior and press the Installed Products button.
You should see the version number of the product you have installed.
 
I have checked with CodeWarrior for HC12 V4.5 and I can create a project for MC9S12E256 there.
 
CodeWarrior for HC12 is pretty similar to CodeWarrior HC08. Only extension are specific to HCS12 core and architecture.
 
CrasyCat
0 Kudos
Reply