CodeWarrior HC16Z1 IDE - Forever Lost?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CodeWarrior HC16Z1 IDE - Forever Lost?

3,644 Views
DavidH
Contributor I
I am looking for a copy of the CodeWarrior HC16Z1 IDE.  I have contacted the support people at Freescale but it seems their archive copy is corrupt.  Does anyone have a copy of the install .exe for this product?  Thank you.
Labels (1)
Tags (1)
0 Kudos
Reply
4 Replies

1,912 Views
CompilerGuru
NXP Employee
NXP Employee
What is exact product name you are looking for?

When I remember right, the last releases supporting the HC16 have been part of a combined installer for multiple processors (HC08, HC11, HC12, HC16,...).

Daniel
0 Kudos
Reply

1,912 Views
DavidH
Contributor I
Daniel,
 
Sorry, I do not have a model or release number.  The following Freescale webpage is all the info I can find.  My copy is corrupt and will not install.  Freescale's archive seems to be corrupt also.  If you have any info on models, releases or combined releases it may help me track down an image with Freescale.
 
 
Best regards,
 
David
0 Kudos
Reply

1,912 Views
CrasyCat
Specialist III
Hello
 
I do not have a web installer for CodeWarrior HC16, but I have an image of CD installer that I could zip and upload on a FTP site.
 
Would that help?
 
CrasyCat
0 Kudos
Reply

1,912 Views
PadelisGR
Contributor III

Hi there!

 

Sorry to bring this up again but is there an FTP that i could get that image file?

I want to write some code for a 68hc16 processor and i need it!

 

Thank you in advance

0 Kudos
Reply