CodeWarrior 5.9.0 for S9S08DZ96F2MLH (File Error 206003)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CodeWarrior 5.9.0 for S9S08DZ96F2MLH (File Error 206003)

1,442件の閲覧回数
chenyu1
Contributor I

When I compile with Codewarrior, I will be prompted to modify the file. How to solve the problem? My chip uses S9S08DZ96F2MLH, the software has been mass-produced software, without any modification directly open the project for compilation will report errors, I have tried to compile on several computers will have this error. I tried to import the project using import again, but File Error 206003 was reported. Check the folder properties and set to read-write, but the problem is still there, please help to see what is the reason, thank you!

 

The error message is as follows:

 

Proect.c

This fie has been nodified outside of the source editor.
Do you want toecad it ?

 

End of main routine wes updated in main module. (Project.c)

 

File Error 206003.
Could not open file because access was denied.

0 件の賞賛
返信
1 返信

1,413件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi chenyu1 

In  a first time check that all the files of your project directory are not in read-only, then is the problem still remains, in your project directory, delete the <nameofyourprojet>_data folder. See if  this could fix your problem.

Have a nice day,

Jun Zhang

0 件の賞賛
返信