Code warrior MCP5200 "Connection Refused".
- 新着としてマーク
- ブックマーク
- 購読
- ミュート
- RSS フィードを購読する
- ハイライト
- 印刷
- 不適切なコンテンツを報告
Hello, we have a problem on programming uC MCP5200 by Codewarrior Tap via SW Codewarrior Mobile GT v9.2. Tap is connected to the workstation PC via Ethernet and we can ping its IP adress and make TELNET connection. When we try to erase the flash memory of the MCP5200 we always get a message from CW Mobil GT v.9.2: "Connection Refused". On the CCS station we saw that logic port 41475 is locked and we can't communicate with the device. Anyone could give us any suggestions? Thanks a lot!


- 新着としてマーク
- ブックマーク
- 購読
- ミュート
- RSS フィードを購読する
- ハイライト
- 印刷
- 不適切なコンテンツを報告
Hi,
CW for MGT v9.2 is old and the CCS driver installed was not compatible with CW TAP interface.
We've a doc giving some information to use CW TAP under MGT.
Please have a look to:
http://cache.freescale.com/files/32bit/doc/app_note/AN4780.pdf
The CCS is not anymore available to the link provided in the doc.
Attached you will find the CCS delivered under MCUv10.6.4 which is one of last CCS version.
Hope this will help you.
Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------