Can Code Warrior IDE version 10.6 be installed in ubuntu?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Can Code Warrior IDE version 10.6 be installed in ubuntu?

3,270 次查看
ddpd
Contributor III

I would like to know if the Code Warrior IDE can be installed in ubuntu 14.04. ?

 

I cannot find any supported downloads for ubuntu. Could anyone please post the link.

 

Thanks in advance

标签 (1)
标记 (3)
0 项奖励
回复
5 回复数

2,840 次查看
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Dino,

The last CodeWarrior version supported in Linux was CodeWarrior 10.2, it can be downloaded from the following page and it supports Ubuntu 10.04:

CodeWarrior Legacy Downloads|NXP

Click on "Evaluation: CodeWarrior for MCU 10.2 Eval (Linux)"

Hope it helps!

Best Regards,

Carlos Mendoza

Technical Support Engineer

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,840 次查看
ddpd
Contributor III

I am using freescale kinetis TRK-KEA128 MCU. I believe Code warrior v10.2 does not support that  MCU.

Is there any other alternative solution other than using windows?

0 项奖励
回复

2,840 次查看
TICS_Fiona
NXP Employee
NXP Employee

Hello Dino

KEA series are supported from CodeWarrior v10.6.

For an IDE supporting Linux OS, you may choose KDS:

http://www.nxp.com/products/software-and-tools/run-time-software/kinetis-software-and-tools/ides-for...

Best Regards

Fiona Kuang

Technical Information & Commercial Support

0 项奖励
回复

2,840 次查看
ddpd
Contributor III

Hi Fiona Kuang,

I have installed KDS, but unfortunately I cannot install KSDK since it doesn't support my evaluation board TRK-KEA128. After using KDS, I have some difficulty in debugging,

1. I cannot see any printf statements in the console.

2. I observed that the interrupt vector number for many peripherals are different when compared with Codewarrior (SKEAZ1284.h)

3. Also the KDS doesn't support my board therefore I created project by selecting the processor unlike the board in Code-warrior. But I feel something is not correct.

Could you please share a working project for TRK-KEA128, so that I can start working on my application.Or Could you please direct me to respective section.

Thanks in advance

0 项奖励
回复

2,840 次查看
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Dino,

Please take a look to the following post that explains how to enable semihosting in KDS. About the working projects, there are some CodeWarrior projects you can use as reference and a document explaining these example projects:

Kinetis KEA128 StarterTRAK CAN Applications|NXP

http://cache.nxp.com/files/microcontrollers/doc/app_note/AN4942.pdf

Hope it helps!

Best Regards,

Carlos Mendoza

Technical Support Engineer

0 项奖励
回复