CW10 and PE USB Multilink on Win7 x64

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CW10 and PE USB Multilink on Win7 x64

3,979 次查看
chuckiethedrago
Contributor I

I am using a PE micro USB Multilink Interface for development on win7x64, and a MC9S08QE8 device.

I can successfully debug, breakpoint etc.

 

My problem is in trying to program the device, using the USB Multilink Interface.

I have tried the Simple Flash tool CW10, but it fails, so I used the Flash Programmer and set up a programming task, and it failed too.

The failed results are shown below:

 

fl::target -lc "MyAlarm_Using_USB_ML"
fl::target -b 0x0 0x0
fl::target -v off -l off -ie on -i "" -p MC9S08QE8
cmdwin::fl::device -d "MC9S08QE8_FLASH" -o "8kx16x1" -a 0xe000 0xffff
cmdwin::fl::erase all
 Beginning Operation ...   
-------------------------
Initializing remote connection ...   
Performing target initialization ...   
Device MC9S08QE8_FLASH   
Detect frequence ...  
Frequence 0 Khz  
 Erasing .............
Error:  Erase Command Failed.  Operation timeout. Protect violation error.
An invalid preference was passed to the GDI protocol plugin(HC GDI Protocol Adapter
Error: Device MC9S08QE8_FLASH

 

Has anybody successfully programmed a device with the PE micro USB Multilink Interface using CW 10?

 

 

Details:

CodeWarrior for MCU
Version: 10.1
Build Id:110204

 

PE Micro USB Multilink Interface

Rev C

USB HCS08/HCS12 MULTILINK detected - Flash Version 5.84

 

Win 7 64 bit

 

Thanks in advance. (tia)

标签 (1)
标记 (1)
0 项奖励
回复
4 回复数

2,248 次查看
J2MEJediMaster
Specialist I

Are you using P&E Microcomputer Systems' 64-bit drivers for the Multilink? They can be downloaded from the web site at www.pemicro.com.

 

---Tom

0 项奖励
回复

2,248 次查看
chuckiethedrago
Contributor I

Hi Tom,

 

Yes it has the correct drivers.

It works for debugging. So it does erase and program in debugging mode.

Using the "flash" function of CW10 is where it fails.

 

I see the problem as a CW -> PE interface, or PE settings problem.

0 项奖励
回复

2,248 次查看
J2MEJediMaster
Specialist I

If you're able to debug the program in RAM, I would think that the CodeWarrior <-> PEMicro interface is working. The flash may be secured accidentally. However, I am also puzzled over that 0 frequency setting. If you haven't already, it's time to file an on-line service request on this. Click here to do that.

 

---Tom

0 项奖励
回复

2,248 次查看
buckeyeman
Contributor III
Did you get this problem sorted out? If so, what was the solution? I am looking at getting a P&E device for communicating with my EVBQE128 board, on WIN 7 64-bit, seeing as how there is not a SofTec 64-bit USB driver that would support the usual USB comm link between that board and CW v10.1.
0 项奖励
回复