CW IDE version 5.7.0 querry regarding Device and Connection

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CW IDE version 5.7.0 querry regarding Device and Connection

ソリューションへジャンプ
3,116件の閲覧回数
Destiny
Contributor I
Dear All
       I am completely new to this MCU world and this CodeWarrior Appliction. The querry I do have is about the derivative we would like to use in device and connections in codewarrior(version 5.7.0). The device I would like to work on is S08EL family (or S08SL )(or even  S08SG)..but unfortunately its not available in the device and connection options. Can anybody help me out with it??
thanks in advanced!!!
Regards
Destiny
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
2,136件の閲覧回数
CrasyCat
Specialist III
Hello
 
Look at  the CodeWarrior for HCS08 Update and Patched web page.
There is a service pack called "CodeWarrior for HC08 v5.1 - EL32 Service Pack ".
 
This package includes support for the MC9S08EL32, MC9S08EL16, MC9S08SL16, and MC9S08SL8 derivatives.
 
There is another service pack called "CodeWarrior for HC08 v5.1 - SG8/SH8 Service Pack "
This package includes support for the MC9S08SH8, MC9S08SH4, MC9S08SG8 and MC9S08SG4 derivatives.
 
Click here to go to the CodeWarrior for HC08 V5.1 update and patches web page.
 
Be careful. You need to run CodeWarrior for HC08 V5.1 to be able to install those patches.
To control which version of CodeWarrior for HC08 you are using:
    - Start CodeWarrior
    - Select Help -> About Freescale CodeWarrior
    - Click on "Install Products"
    - CodeWarrior version used is displayed on top in the Installed Products dialog.
CrasyCat

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,137件の閲覧回数
CrasyCat
Specialist III
Hello
 
Look at  the CodeWarrior for HCS08 Update and Patched web page.
There is a service pack called "CodeWarrior for HC08 v5.1 - EL32 Service Pack ".
 
This package includes support for the MC9S08EL32, MC9S08EL16, MC9S08SL16, and MC9S08SL8 derivatives.
 
There is another service pack called "CodeWarrior for HC08 v5.1 - SG8/SH8 Service Pack "
This package includes support for the MC9S08SH8, MC9S08SH4, MC9S08SG8 and MC9S08SG4 derivatives.
 
Click here to go to the CodeWarrior for HC08 V5.1 update and patches web page.
 
Be careful. You need to run CodeWarrior for HC08 V5.1 to be able to install those patches.
To control which version of CodeWarrior for HC08 you are using:
    - Start CodeWarrior
    - Select Help -> About Freescale CodeWarrior
    - Click on "Install Products"
    - CodeWarrior version used is displayed on top in the Installed Products dialog.
CrasyCat
0 件の賞賛
返信
2,137件の閲覧回数
Destiny
Contributor I
Dear CrasyCat
    Thanks a lot for your valuable help.
Regards
Destiny
0 件の賞賛
返信