CW 6.1 evaluation linker code size limitation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CW 6.1 evaluation linker code size limitation

ソリューションへジャンプ
4,998件の閲覧回数
Kerem
Contributor II
Hi,
 
Is there a code size limitation on CW 6.1 evaluation version for RS08KA. I have developed a small C application in C and had it compiled successfully. But the linker issues a fixup error message for some functions. When commented, the code size reduces and linker completes with no errors.
 
Thanks,
 
Kerem
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
3,230件の閲覧回数
Kerem
Contributor II
Hi Daniel,
 
I found the reason. Like you said it was not about code size limitation. hidef.h needed to be included before peripheral definitions.
 
Thanks,
 
Kerem

元の投稿で解決策を見る

0 件の賞賛
返信
6 返答(返信)
3,230件の閲覧回数
CompilerGuru
NXP Employee
NXP Employee
A fixup overflow has nothing to do with the C code size limitation.
If you get such an error you are probably doing something which just should not work....

The most common bug for the HC08 which causes a fixup overflow is to declare a variable to be in the zero page, but then not actually allocating it in the first 256 bytes of the memory.

Another one is to map .text into multiple segments, that can cause a fixup overflow but there is a compiler option
(I think the option is mentioned in the default prm, just done remember it for sure) to disable the short branch optimization (that's the one which may cause a fixup overflow if he code is distributed into multiple segments).

Daniel
0 件の賞賛
返信
3,230件の閲覧回数
CompilerGuru
NXP Employee
NXP Employee
Ups, the OP was for the RS08 and not for the HC08. Anyway, it still has nothing to do with the license. I think the code limits are smaller for the RS08, but non the less, fixup overflows are only caused by how the code/variables are allocated and not by how much code there is.
The RS08 also has some special memory areas, not sure if it has a short branch optimization, but for a RS08 I think it is less common to distribute the code into multiple segments anyway.
The simplest thing would be probably when you copy paste the linker error here, the message window does support CTRL-C.

Daniel
0 件の賞賛
返信
3,230件の閲覧回数
Kerem
Contributor II
It appears not related to variables. It is something about code. Here is the message
 
Link Error   : L1907: Fixup overflow in set2sqr, to _xxPSID17 type 1, at offset 0x1D

Link Error   : Link failed
 
Compile process is ok. I left the optimization setting as default. Linker file contains contiguous flash & ram memory. Below is the link file contents as well.
 
First time using this suite, so not quite familiar with the options. My parts is R08KA08 which has 8k flash and some 200 byte ram.
 
Kerem
 
NAMES END /* CodeWarrior will pass all the needed files to the linker by command line. But here you may add your own files too. */
SEGMENTS /* Here all RAM/ROM areas of the device are listed. Used in PLACEMENT below. */
    TINY_RAM                 =  READ_WRITE   0x0005 TO 0x000D;
    RAM                      =  READ_WRITE   0x0030 TO 0x00BF;
    RESERVED_RAM             =  NO_INIT      0x0000 TO 0x0004;
    ROM                      =  READ_ONLY    0x2000 TO 0x3FF7;
END
PLACEMENT /* Here all predefined and user segments are placed into the SEGMENTS defined above. */
    RESERVED                 INTO RESERVED_RAM;
    TINY_RAM_VARS            INTO TINY_RAM;
    DIRECT_RAM_VARS          INTO RAM, TINY_RAM;
    DEFAULT_RAM              INTO RAM, TINY_RAM;
    DEFAULT_ROM              INTO ROM;
END

STACKSIZE 0x00 /* no stack for RS08 */
VECTOR 0 _Startup /* Reset vector: this is the default entry point for an application. */
0 件の賞賛
返信
3,230件の閲覧回数
CompilerGuru
NXP Employee
NXP Employee
What is set2sqr? Is this a C or an assembly function (or even a constant?)
The simplest way is to open the source file it is defined in and use the disassemble contect menu.
That is at offset 0x1D?

Daniel
0 件の賞賛
返信
3,231件の閲覧回数
Kerem
Contributor II
Hi Daniel,
 
I found the reason. Like you said it was not about code size limitation. hidef.h needed to be included before peripheral definitions.
 
Thanks,
 
Kerem
0 件の賞賛
返信
3,230件の閲覧回数
Kerem
Contributor II
set2sqr is a C function like the rest of the code. I'm trying to find the source of the error. If I remove set2sqr then the linker issues same message for main. Then after gradually deleting the code lines of main, at some point (I presume my evaluation version has a limitation) linker completes with no error.
 
CW 6.1 does not mention RS08KA8 support (8K flash part). Instead, I can only see RS08KA2 in the device selection menus. And that part has 2K flash. Presumably the linker allows half of RS08KA2's flash capacity of 1024 bytes.
 
Right now I'm trying to generate a header file which includes peripheral definitions for KA8 part. I'll be able to investigate more in an hour.
 
Kerem
0 件の賞賛
返信