CW 10.4 editor & include browser display problem for PXS30_Tower project. Operator error?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CW 10.4 editor & include browser display problem for PXS30_Tower project. Operator error?

2,858件の閲覧回数
paul_murray
Contributor II

Is anyone else seeing this issue?

 

    The PXS30_Tower project defines two Project Configuration options:

    PXS3020_INTERNAL_RAM and PXS3020_INTERNAL_FLASH. The Prefix subdirectory

    has an include file for each.

 

    PXS3020_INT_FLASH_VLE_DPM.prefix contains '#define ROM_VERSION 1',

    PXS3020_INT_RAM_VLE_DPM.prefix has no define for ROM_VERSION.

    So...

 

    If I select PXS3020_INTERNAL_RAM as my Project Configuration and open

    PRC1_Sources/_start_p1.c and look at line 110, I see a conditional

    block grayed-out as expected, because ROM_VERSION is not defined by

    PXS3020_INT_RAM_VLE_DPM.prefix. So good so far.

 

    However, if I select PXS3020_INTERNAL_FLASH and look at line 110 of

    _start_p1.c, the preprocessor block remains grayed-out.

    If I open an 'Include Browser' window and drop _start_p1.c into it,

    the first file listed is PXS3020_INT_RAM_VLE_DPM.prefix. This is true

    for either Project_Configuration.

 

    NB: This is simply a viewing problem; the builds include the correct

    prefix files and generate the correct code. There is probably a simple

    fix?

 

 

 

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,754件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

it looks like a CW IDE problem. can you please upload the demo project here, so that we can reproduce and confirm it?

0 件の賞賛
返信

2,754件の閲覧回数
paul_murray
Contributor II

Thanks for your response.  It would be interesting to see if you get (as I suspect) the same behavior with the vanilla software packaged with cw10.4.

I'll be glad to upload my (slightly modified) demo, but can't find upload packaging instructions.  I know I've seen them, but can't find then this morning.  Any suggestions?

0 件の賞賛
返信