CodeWarrior開発ツールのナレッジベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CodeWarrior Development Tools Knowledge Base

ラベル
  • General 75

ディスカッション

ソート順:
The content is to tell user how to add nand flash(MT29F2G08ABBDA) support in CW 10.3.
記事全体を表示
In many of user applications we use a CRC/checksum to verify that the code/flash on the target is not modified. For this, not only the code/data in flash counts, but as well all the unused gaps in the memory map. Instead to leave it up to the flasher/debugger (which usually erases it to 0xFF), I want to fill it with my pattern. For example 0xAA.   How to implement? There may be several ways,  but I think the easiest way is to modify linker file.   the linker file structures are different for different MCUs.   For example, CW for 8bit/16bit and Coldfire V1 uses PRM file;  while CW for kinetis Gnu compiler uses ld file. We will talk about each of the case separately. 1. CW for 8bit/16bit and Coldfire V1. 1.1 .  NO FILL command involved. We define a segment  in prm file MYCONST_ROM     =  READ_ONLY    0x0870 TO 0x08FF; Then allocate MYCONST  into it inside PLACEMENT. MYCONST    INTO  MYCONST_ROM; In C code, we only define  my_const_var(0xCCDD) at this range. #pragma CONST_SEG MYCONST const unsigned int my_const_var = 0xCCDD; #pragma CONST_SEG DEFAULT   After build, we will see only 0xCCDD in this area in generated s19 file: S1050870CCDDD9   1.2  use FILL command to fill unused area of MYCONST_ROM With FILL command we can fill unused area of a section.  Add “FILL 0xAA” : MYCONST_ROM       =  READ_ONLY 0x0870 TO 0x08FF FILL 0XAA;   Rebuild the project. we will see the rest of the field of MYCONST_ROM  is filled in  S19 file: S1230870CCDDAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAACF S1230890AAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAA04 S12308B0AAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAE4 S12308D0AAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAC4 S11308F0AAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAA54 2. CW for kinetis GNU compiler: 2.1 . No fill() command involed. Define segment in MEMORY section: my_section    (rx) : ORIGIN = 0X00000800, LENGTH = 0x20   define output  SECTION: .myData : {     . = ALIGN(4);           KEEP(*(.myData))     . = ALIGN(4); }> my_section In C code, define const variable “my_const” (0xCCCCDDDD) const int my_const __attribute__((section(".myData"))) = 0xCCCCDDDD;   After build, we will see only 0xCCCCDDDD in this area in generated s19 file: S1070800DDDDCCCC9E 2.2 Use FILL(0xaa)  command to fill unused area of my_section with 0xAA. Here is the modified code in ld file, I highlight the code I add: .myData : {        . = ALIGN(4);                   KEEP(*(.myData))     . = ALIGN(4);     FILL(0xaa)     . = ORIGIN(my_section) + LENGTH(my_section) ;   }> my_section Rebuild the project. we will see the rest of the field of my_section is filled with 0xAA in  S19 file: S1130800DDDDCCCCAAAAAAAAAAAAAAAAAAAAAAAA9A S1130810AAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAA34
記事全体を表示
This document contains an overview of what is the Codewarrior Linker File for Kinetis devices and how to edit it to relocate code and data. It also explains how to create a debug sesion out of external RAM.   Regards, Carlos
記事全体を表示
This is a test for 56F800EX new additional 32bit multiplication instructions on CodeWarrior V10.3/V10.5/V10.6.
記事全体を表示
How to install and use eGit plug-in in CodeWarrior
記事全体を表示
This document describes the steps required for U-Boot debugging using the CodeWarrior IDE for low-end and high-end Power Architecture CPU, from NOR, NAND, SPI and SD card flash devices.
記事全体を表示
CodeWarrior MCU 10.5 for Kinetis KV10   To setup your CodeWarrior development environment for Kinetis KV10 applications. Read the documents attached for download and installation instructions. Download and install the CW MCU v10.5  product, patch and service pack in the order specified:   Evaluation: CodeWarrior for Microcontrollers 10.5 (Eclipse, Offline) CW MCU v10.5 PEx MQX Lite Update 1.0.1 CW MCU v10.5 Kinetis KV10 75MHz Service Pack   the updates were just posted on the following URLs: http://www.freescale.com/webapp/sps/site/overview.jsp?code=CW_UPDATES_MCU_10_5
記事全体を表示
T1040 is new to all the customers. The ecosystem is still not mature in this moment in Jan'2014 The note is for someone who is using Codewarrior PA10.3.3 for T1040 platform board bring up or debugging on this moment. if you have problem to connect T1040 platform with Codewarrior, the document might help you.
記事全体を表示
Detailed analysis report, done by Micetek (Freescale subcontractor that manufactures USB TAPs), following incidents where Rev F USB TAP/COP units were failing.
記事全体を表示
If you would like to migrate a project which is created by classic CW to eclipse CW, this file illustrates one of the ways to import PE beans to eclipse IDE manually. Test environment: 56F8037 in CW for DSC V8.3, CW for MCU V10.3, CW for MCU V10.4.
記事全体を表示
Another attachment in thead
記事全体を表示
I just download FNET2.5.0, it can't debug it by CW10.4, it comes error message when I start debug "Could not open memory configuration file".   The CW10.4 works for other examples project.   Why?   Regards Sam
記事全体を表示
Scanboard is a tcl proc within the IDcode.tcl script that can be used as a quick sanity check for basic JTAG connectivity. This routine will return the JTAG ID codes for devices on the scanchain and if they are known Freescale devices (at the time the script was last updated) the core indexes will also be displayed for CodeWarrior project configuration. IDcode.tcl is included automatically during the CodeWarrior installation but updates may be available.   This script is executed within the CodeWarrior Connection Server (CCS) and not the CodeWarrior IDE itself where ccs is the conduit that the CodeWarrior Debugger talks to the TAP hardware. CCS can also be used standalone but this is not a supported mode and the use of it is not documented.   On a windows machine start ccs via the Start menu for the CodeWarrior installation you wish to use.   i.e. Start → All Programs → Freescale CodeWarrior →CW for Power Architecture v10.2.1→ CodeWarrior Connection Server   CCS starts iconized in the task bar so double click on the icon to display the ccs console window   On a Linux machine start ccs manually via the ccs executable location within the CodeWarrior installation directory ($CW_INSTALLDIR)/PA/ccs/bin/ccs   i.e. /usr/local/Freescale/CodeWarrior_PA_10.2.1/PA/ccs/bin/ccs Once the CCS console is available the IDcode.tcl file must be brought into the tcl environment via the source command. Beware that on a Linux system the file name is case sensitive.   % source IDcode.tcl   The script will automatically query the host system to determine if there are any available CodeWarriorTAP or USBTAP devices connected via USB which can be used for a remote connection. Specify the connection option that is attached to the target system. For example to configure the connection to be a CodeWarriorTAP on the network select 2 and then enter the IP address or the CodeWarriorTAP name if it is in the host table or can be found within the DNS tables.   It is also possible to predefine custom remote connections via the DefinedCCSConnections.tcl located within the …/ccs/bin directory as well. See this file for details. Once the remote connection has been specified the script will the automatically execute the scanboard proc and attempt to read back the IDcode(s) available on the JTAG scanchain.     In this example the CodeWarriorTAP is connected to a system that has a T4240 processor and displays the IDcode for this device. If there had been multiple processors available on the scan chain each device would have been identified and displayed.
記事全体を表示
If you mix the great new TAP kit for CodeWarrior with the right Tip, the possibilities of debugging your devices become bigger and more powerful. In this occasion I will show you one more removable probe Tip: the CWH-CTP-BDM-YE, meant for ColdFire processors connects your ColdFire microprocessor/microcontroller target system’s BDM port to the CodeWarrior TAP base unit’s 30-pin target connector.   The compatibility of this Tip and the CodeWarrior TAP CWH-CTP-BASE-HE base unit empowers your creations and helps you lowering costs. Note this Tip is not included within the TAP kit. Check out the cool features:   Features Removable probe tip Low cost and economical to order several spares Allows base unit to work with several different target types   System Requirements ColdFire based target system with BDM header CodeWarrior TAP  
記事全体を表示
You remember the previous post regarding the new awesome TAP for CodeWarrior applications?   Today I'd like you to meet this device shown up here. Is the CWH-STC-COP-YE, a removable probe tip for StarCore and DSC processors. This probe tip connects your StarCore or DSC processor target system’s ONCE port to the CodeWarrior TAP base unit’s 30-pin target connector.   And of course this tip is compatible with the CodeWarrior TAP previously mentioned (CWH-CTP-BASE-HE). As a matter fact, the base unit doesn't come with a probe tip, so it is necessary to acquire one of the tips available to debug your device. Check out the main features!   Features Removable probe tip Low-cost and economical to order several spares Allows base unit to work with several different target types System Requirements StarCore or DSC target system with ONCE header CodeWarrior TAP  
記事全体を表示
Hey there! Are you familiar with this device shown on top? If you find it similar to the CodeWarrior TAP probe then you are ringing the right bells.   The magic thing of this innovative device is that you can debug systems remotely or more effectively share a single system with multiple developers. When a shared system is not needed, CodeWarrior TAP connects directly to the developer’s workstation with a single USB cable. Power is supplied by the USB port so that no additional cables are required!   This means that the TAP also enables Freescale target system debugging via a standard debug port (usually JTAG) while being connected to your workstation via Ethernet or USB. For this reason this device can also be found under the name of probe, JTAG probe, JTAG emulator or target probe.   These are some of the great features offered by the TAP: Allows either USB or Ethernet (10/100 ) host connection for the developer workstation USB powered, even when using Ethernet Low cost removable probe tips sold separately Supports debugging via JTAG interface Automatically supports system voltage levels from 1.2 to 3.3 Supports all available core speeds and voltages for supported Freescale processors As a convenience feature, the CodeWarrior can connect to a target systems serial port allowing telnet access to a remotely located system and control of the U-boot program.   Keep finding more features and applications within the Fact Sheet If you'd like to dig further into the TAP world, you can also find The User Guide equally useful!      Please note that this device is not up for sale (just yet!). Regardless, Freescale is accepting pre-orders for CodeWarrior TAP now with shipments planned in late October, and DebuggerGuys will keep you informed on this! Don't hesitate on asking beyond!      
記事全体を表示