In many of user applications we use a CRC/checksum to verify that the code/flash on the target is not modified. For this, not only the code/data in flash counts, but as well all the unused gaps in the memory map. Instead to leave it up to the flasher/debugger (which usually erases it to 0xFF), I want to fill it with my pattern. For example 0xAA. How to implement? There may be several ways, but I think the easiest way is to modify linker file. the linker file structures are different for different MCUs. For example, CW for 8bit/16bit and Coldfire V1 uses PRM file; while CW for kinetis Gnu compiler uses ld file. We will talk about each of the case separately. 1. CW for 8bit/16bit and Coldfire V1. 1.1 . NO FILL command involved. We define a segment in prm file MYCONST_ROM = READ_ONLY 0x0870 TO 0x08FF; Then allocate MYCONST into it inside PLACEMENT. MYCONST INTO MYCONST_ROM; In C code, we only define my_const_var(0xCCDD) at this range. #pragma CONST_SEG MYCONST const unsigned int my_const_var = 0xCCDD; #pragma CONST_SEG DEFAULT After build, we will see only 0xCCDD in this area in generated s19 file: S1050870CCDDD9 1.2 use FILL command to fill unused area of MYCONST_ROM With FILL command we can fill unused area of a section. Add “FILL 0xAA” : MYCONST_ROM = READ_ONLY 0x0870 TO 0x08FF FILL 0XAA; Rebuild the project. we will see the rest of the field of MYCONST_ROM is filled in S19 file: S1230870CCDDAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAACF S1230890AAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAA04 S12308B0AAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAE4 S12308D0AAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAC4 S11308F0AAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAA54 2. CW for kinetis GNU compiler: 2.1 . No fill() command involed. Define segment in MEMORY section: my_section (rx) : ORIGIN = 0X00000800, LENGTH = 0x20 define output SECTION: .myData : { . = ALIGN(4); KEEP(*(.myData)) . = ALIGN(4); }> my_section In C code, define const variable “my_const” (0xCCCCDDDD) const int my_const __attribute__((section(".myData"))) = 0xCCCCDDDD; After build, we will see only 0xCCCCDDDD in this area in generated s19 file: S1070800DDDDCCCC9E 2.2 Use FILL(0xaa) command to fill unused area of my_section with 0xAA. Here is the modified code in ld file, I highlight the code I add: .myData : { . = ALIGN(4); KEEP(*(.myData)) . = ALIGN(4); FILL(0xaa) . = ORIGIN(my_section) + LENGTH(my_section) ; }> my_section Rebuild the project. we will see the rest of the field of my_section is filled with 0xAA in S19 file: S1130800DDDDCCCCAAAAAAAAAAAAAAAAAAAAAAAA9A S1130810AAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAA34
查看全文