please help..i am not able to flash a file(.afx) to target .it is giving some internal error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

please help..i am not able to flash a file(.afx) to target .it is giving some internal error

1,840 次查看
maheshgupta
Contributor I

please help..i am not able to flash a file(.afx) to target .it is giving some internal error

标签 (1)
0 项奖励
回复
2 回复数

1,678 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

you can use simple flash tool to flash afx file to target, see

Standalone Flash Programmer | MCU on Eclipse

it's for download s19 file but the method is the same for afx file.

if above can not help. to solve your problem, we need:

1. your CW version info.

2. error message screenshot

3. what chip do you work with?

4. can you successfully download a project to chip via debugger?


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,677 次查看
maheshgupta
Contributor I

Dear ZhangJennie,

Thank you for your quick response. Below are the details required by you :

CW Version : CodeWarrior for MCU ,Version: 10.5, Build Id:130916

Microcontroller : PK60N512VMD100

We are able to flash our code through debugger.

PFA for error screenshot and diagnostic report generated during flashing

code.

Mahesh Gupta,

Dy.Manager,

Bharat Electronics Ltd.

Ministry of Defense

ZhangJennie

replied to the discussion

"please help..i am not able to flash a file(.afx) to target .it is giving

some internal error"

To view the discussion, visit:

https://community.freescale.com/message/600327?et=watches.email.thread#600327

>

0 项奖励
回复