interrupt  for inputcapture mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

interrupt  for inputcapture mode

3,078 Views
kdn
Contributor III

which interrupt I have to enable in CPU to get interrupt on input capture mode .

Labels (1)
0 Kudos
Reply
2 Replies

2,913 Views
trytohelp
NXP Employee
NXP Employee

Refer to

      https://community.freescale.com/thread/338349


Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,913 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi KDN,

I suggest you use Capture component and refer demo code under

C:\Freescale\CWS12V5_1\ProcessorExpert\Projects\Test projects\Capture

Best Regards,

Zhang Jun

=====================================================

this answer is for you. if it helps, please click on "Correct Answer " button. Thanks!

======================================================

0 Kudos
Reply