i've lost the ability to set breakpoints. when i attempt to set, i see the little icon indicating a breakpoint but it's got a slash across it and execution won't stop

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i've lost the ability to set breakpoints. when i attempt to set, i see the little icon indicating a breakpoint but it's got a slash across it and execution won't stop

1,061 Views
danielfreepons
Contributor I

- CodeWarrior for MCU

     Version: 10.5

     Build Id:130916

 

i'm able to stop execution by clicking the 'pause' button

Labels (1)
0 Kudos
Reply
1 Reply

996 Views
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Daniel,

I think that the following post created by our colleague Erich Styger might be helpful for you, it explains the difference between software and hardware breakpoints and what to do when you run out of hardware breakpoints:

Software and Hardware Breakpoints | MCU on Eclipse

Hope it helps!

Best Regards,

Carlos Mendoza

Technical Support Engineer

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply