copy project

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

copy project

1,789 Views
edsonabreu
Contributor I

Hi!

 

     I would like to copy the project and rename it to another code. With this I can generate other files for another versions of the product.

     With CodeWarrior ¨it was easier to do this.

     I saw in this forum the same doubt but I didn't understand tha solution.

     All way that I tried, when I build the project, the result is some file tied to the previous one.

     Anyone knows an easier way to do this?

 

Thanks a lot

 

Edson

Labels (1)
0 Kudos
Reply
2 Replies

1,672 Views
edsonabreu
Contributor I

Thanks a lot for your suggestion but I decided to create a new one and import Board Configuration setup. The text of the Processorexpert.c and events.c was copied too.

In this way I think it easier than the procedures in the links.

Edson

0 Kudos
Reply

1,672 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Edson:

Copying a project is a complicated procedure. Take a look at the next 2 tutorials by our colleague Erich Styger:

Copy my Project | MCU on Eclipse

Copy my CodeWarrior Project | MCU on Eclipse

Hope this helps!

Jorge Gonzalez

0 Kudos
Reply