codewarrior tap and codewarrior usb tap

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

codewarrior tap and codewarrior usb tap

2,611件の閲覧回数
威杨
Contributor III

Hi

   I use codewarrior usb tap a long time, my board chip is MPC8309.i use it to download uboot, my hardware not support jumper,everytime througt download the 8309SOM_HRCW_jtag.txt file, like this we use a year.

unfortunately the usb tap is broken.i buy a codewarrior tap,but it can't work, i only modify hardward jumper can download uboot,but my board don't obligate the hard jumper.i want to know need to modify what configures the codewarrior tap can working normal, i always think the new must be compatible old functions.please give me some helps.

Thanks.

0 件の賞賛
返信
2 返答(返信)

2,392件の閲覧回数
Pavel
NXP Employee
NXP Employee
  1. Install please Software Patch: CW PA v8.8.6 Windows - Patch. This path contains new version CCS driver for CodeWarrior TAP supporting.
  2. Reinstall ccs USB driver using the following files:

C:\Program Files (x86)\Freescale\CodeWarrior PA V8.8\ccs\drivers/ccs_drivers_installation_help.txt

 

and

 

C:\Program Files (x86)\Freescale\CodeWarrior PA V8.8\ccs\drivers\usb\readme.txt


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,392件の閲覧回数
威杨
Contributor III

Thanks for your help

0 件の賞賛
返信