code warrior DSC V8.3 special edition in windows 8 64 bit

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

code warrior DSC V8.3 special edition in windows 8 64 bit

1,592件の閲覧回数
arunrajk
Fresh Out Contributor

I installed code warrior DSC V8.3 special edition in windows 8 64 bit  i can't open the processor expert component wizard. any one suggest me the solution.

0 件の賞賛
返信
1 返信

1,452件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

according to CodeWarrior Factsheet, http://www.nxp.com/docs/en/fact-sheet/950-00437.pdf 

processor expert component wizard is not available in CodeWarrior for DSC.

Besides, CodeWarrior for DSC v8.3 doesn't support  64bit win8, it supports "Windows® XP/Vista 32-bit (Home Premium Edition & Business Edition)", if you want to wort with DSC, please use CW v10.7 instead.

CodeWarrior for Microcontrollers-Eclipse IDE|NXP 


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信