What is the difference between MT29FxG08-IFC_64b.bin and MT29FxG08-IFCv1_64b.bin

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What is the difference between MT29FxG08-IFC_64b.bin and MT29FxG08-IFCv1_64b.bin

ソリューションへジャンプ
3,410件の閲覧回数
Johnson_s
Contributor III

I am creating the necessary device files to add a new NAND device.

In the XML file within the algorithms folder, there is a section where a binary file is specified.

When I specify MT29FxG08-IFCv1_64b.bin, it reads and writes successfully, but when I specify MT29FxG08-IFC_64b.bin, I get a [FP: operation timeout] error.

What is the difference between these binary files?

0 件の賞賛
返信
1 解決策
3,296件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please use MT29FxG08-IFCv1_64b.bin, this is the latest and correct version.

Please refer to the following in LS1043A_RDB_init.py

# Add NAND device
if BOARD_REV_PD:
fl.add_device({"alias": "nand", "name": "MT29F4G08ABBFAv1", "address": 0x7E800000, "ws_address": 0x10000000, "ws_size": 0x1FFFF, "geometry": "8x1", "controller": "IFC"})
else:
fl.add_device({"alias": "nand", "name": "MT29F4G08ABBDAv1", "address": 0x7E800000, "ws_address": 0x10000000, "ws_size": 0x1FFFF, "geometry": "8x1", "controller": "IFC"})

We also use algorithm MT29FxG08-IFCv1_64b.bin on NXP demo board.

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
3,297件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please use MT29FxG08-IFCv1_64b.bin, this is the latest and correct version.

Please refer to the following in LS1043A_RDB_init.py

# Add NAND device
if BOARD_REV_PD:
fl.add_device({"alias": "nand", "name": "MT29F4G08ABBFAv1", "address": 0x7E800000, "ws_address": 0x10000000, "ws_size": 0x1FFFF, "geometry": "8x1", "controller": "IFC"})
else:
fl.add_device({"alias": "nand", "name": "MT29F4G08ABBDAv1", "address": 0x7E800000, "ws_address": 0x10000000, "ws_size": 0x1FFFF, "geometry": "8x1", "controller": "IFC"})

We also use algorithm MT29FxG08-IFCv1_64b.bin on NXP demo board.

0 件の賞賛
返信
3,378件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi  Johnson_s,

What's your chip part number?

Thanks,

Jun Zhang

0 件の賞賛
返信
3,368件の閲覧回数
Johnson_s
Contributor III

I can't provide details, but it's the MT29 series.

0 件の賞賛
返信
3,358件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Johnson_s 

We need to know which MCU/MPU device you are using in combination with MT29?

Thanks,

Jun Zhang 

0 件の賞賛
返信
3,356件の閲覧回数
Johnson_s
Contributor III

I'm sorry, I misunderstood. I am using the LS1046A.

0 件の賞賛
返信