Unable to download Code on MPC555

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to download Code on MPC555

1,735 Views
hana
Fresh Out Contributor

Hii all,


I have problem to download Code onto the MPC555 either on

RAM or Flash using CodeWarrior.

CodeWarrior version 8.7 and my PC is XP 2002 SP3.

 

 

when trying to download the Hello project on RAM I got this

error. >> *pic (ram_error)*.

 

Inline image 1

 

and when trying to set the Flash setting, then need to erase step(from

manual), I couldn't get connect to MPC555 and I have error but without

description; as in the *pic (flash_error)*.

Inline image 2

 

Also when trying to download Code onto MPC555 using MATLAB via Serial

ports, I have this error; *pic (com_error)*.

 

Inline image 1

 

Note here that I have used the serial ports and got successful downloading

before many times, BUT suddenly it isn't able to download and always give

the Com error, although I haven't change any thing to the

port,configurations and jumper setting.

Don't know why!

 

 

Please, any help toward this urgent problem?

 

 

Regards,

Labels (1)
0 Kudos
Reply
1 Reply

1,571 Views
qiaoqiao
Contributor I

Hi, hana Ahmad AL-Theiabat,

Do you figure out this problem?

I also face this problem too. If you have some sultion to this problem.

Could you let me know? I am very please if you can answer me through board or through my email: [email protected].

Thanks,

yeqin 

0 Kudos
Reply