To use correct  FlexBus  in not multiplexed mode  for  MCF5475

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

To use correct  FlexBus  in not multiplexed mode  for  MCF5475

1,154件の閲覧回数
pierluigirosset
Contributor I

Hi team,

 

my customer Larimart would like an easy HW question about the as and type connection more correct  on the MCF5475 to implement, in order to FlexBus not multiplexed mode.

 

In fact  in the user Manual at the section 2.2.6.3 is described as to use the port FlexBus AD  and PCIAD in not multiplexed mode, but only described.

 

Now my customer would like  be sure the right connections by flash/SRAM/FPGAs.

 

Exist an  Application note , or raccomandations for connections by these devices... if exist a schematic will be fantastic. ?

thank a lot

Pierluigi

ラベル(1)
0 件の賞賛
返信
0 返答(返信)