There is no processor menu for choice while create a QorIQ Configuration Project

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

There is no processor menu for choice while create a QorIQ Configuration Project

2,139 Views
flydick
Contributor I

There is no processor menu for choice while create a QorIQ Configuration Project

Installed Products:
 - CodeWarrior for Power Architecture
     Version: 10.5.1
     Build Id:160128

and

 

error Description:Processor Expert configuration file not found or corrupted (PE[_??].cfg).

0 Kudos
Reply
1 Reply

2,068 Views
ufedor
NXP Employee
NXP Employee

It is needed to completely uninstall and re-install the CodeWarrior.

It could be convenient to disable antivirus software for the CW installation period.