The Debugger can not connect to the P&E device.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The Debugger can not connect to the P&E device.

Jump to solution
8,666 Views
adrien_segura12
Contributor I

Hi !

I'm new on Codewarrior and i use a Universal Multilink (Farnell 2315740) to load my projects.

after a trip to make my project work on an other computer with the multilink, i tried to load my 

project on my work computer. And then codewarrior send me this error :

Launching has encountered a problem.

ARM GDI Protocol Adapter : Can't connect. The Debugger can not connect to the P&E device.

I saw that i got the same problem if i diconnect the multilink. but, it seems to work, both leds (orange and blue) 

are on, and i re-installed my drivers and codewarrior .

I noticed that this error occured not only on codewarrior.

Anyone has an idea of how to solve this problem?

Thanks for reading me !

0 Kudos
Reply
1 Solution
8,432 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Adrien,

I suggest you refer this check list to shoot trouble:

Debugging Failure: Check List and Hints | MCU on Eclipse 


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
5 Replies
8,432 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Adrien Segura ,

Please send us more information about your query:

1. Do you use demo board or customized board? part number?

2. Your CW version?

Have a nice day,

Jun Zhang

0 Kudos
Reply
8,432 Views
adrien_segura12
Contributor I

Hi,

thanks for your reply ! I use CodeWarrior V 10.6.4,

my card is customized and used for a bus communication application.

I re-tried to use the multilink on other computer and other applications, it seems that i always have the same error message :

ARM GDI Protocol Adapter : Can't connect. The Debugger can not connect to the P&E device.

 

Any ideas? thanks for your answers !

0 Kudos
Reply
8,433 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Adrien,

I suggest you refer this check list to shoot trouble:

Debugging Failure: Check List and Hints | MCU on Eclipse 


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
8,432 Views
adrien_segura12
Contributor I

Thanks ! the problem is resolved ! 

To all people who have the same problem, the link upside is perfect !

Thank you again ZhangJennie, it was a hardware problem, but the steps of the link you gave were really helpful.

0 Kudos
Reply
8,432 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

You are welcome!

0 Kudos
Reply