TWR-S08LL64 - There is no current communication with the hardware?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

TWR-S08LL64 - There is no current communication with the hardware?

5,940 次查看
JAllen
Contributor I

Hello All,

I recently puchased a used TWR-S08LL64.  Downloaded and installed Codewarrior 6.3. opened PE_LL64_Quick_Start.MCP, opened LL64_Demo.c, and then clicked on Project>Debug
as per directons in the Quick Start Guide.  Got error message " There is no current communications with the hardware."  How can I esablish communication with the TWR-S08LL64 board.  The windows drivers are installed and the board, when connected via the usb port, has two LEDs lit and displays time starting at 6:05 AM on the LCD.

 

Thanks,

 

John Allen.

 

P.S. This is my first post, so I'm not very familiar with how the forum works.

标签 (1)
标记 (2)
0 项奖励
回复
9 回复数

5,577 次查看
trytohelp
NXP Employee
NXP Employee

Hi John,

It seems you've contacted our support team through the SR 1-1270444217.

+++++++++++++++++++

The “.mcp” project files can only work on Classic CodeWarrior for MCUs, not with Eclipse CodeWarrior v10.x.

If you do not have the DVD provided with your tower system I recommend you to download the special edition of classic CodeWarrior v6.3 from the next link, and also the necessary service pack for your LL64 device, which is under “Updates and patches”:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-MICROCONTROLLERS&fpsp=1&tab=Design...

+++++++++++++++++++

Now you've installed  CW for MCU V6.3.

To investigate the problem we need more details:

      - what is the Windows OS ?

      - what is the interface ?

            sample micro USB or Multilink Universal ?

Is there an issue with the driver ?

you could have an issue with the driver version installed.

I found questions/problems about this problem.

Can I recommend you to have a look to the web site:

      http://www.pemicro.com/osbdm/

You can download new driver and found some information regarding OSBDM.

Regards

Pascal

0 项奖励
回复

5,577 次查看
JAllen
Contributor I

1. Connected Twr-S08LL64 to the PC via the usb cable.

2. Pushed button #2.

3. Started CodeWarrior 6.3.

4. Opened file PE_LL64_Quick_Start.mcp.  No errors noticed.

5. Opened file LL84_Demo.c.  No errors noticed.

6. Clicked on Project > Debug and got the following error messages:

+Cpu

  +ERROR: There are errors in this component, it is impossible to generate code

+Cpu

  +ERROR: Error in the component setting. More details provided by Component Inspector for this component

How do I find the errors?

Thanks,

John Allen

0 项奖励
回复

5,577 次查看
trytohelp
NXP Employee
NXP Employee

Hi John,

the MCUinit.c file is generated by Processor Expert.

following the info you provided I think there is a problem with the project or with installation.

I don't have the board on my side but it seems you've a problem to build the application now.

the problem:

+Cpu

  +ERROR: There are errors in this component, it is impossible to generate code

+Cpu

  +ERROR: Error in the component setting. More details provided by Component Inspector for this component

Is generated when processor Expert code is generated.

something seems to be wrong in the Processor Expert config.

By default you should have the info in the bean.

If you can not determine where is the problem, please can you provide me the project ?

    -> zip the full project folder

Pascal

0 项奖励
回复

5,577 次查看
JAllen
Contributor I

Pascal,

Being a novice at using the Forum, I used "Create" to upload the zipped file "twrll64.zip" to the Freescale Community.  I don't know how to send it directly to you.

Thanks again,

John Allen

0 项奖励
回复

5,577 次查看
trytohelp
NXP Employee
NXP Employee

John,

Do you want to keep the project "private" ?

      not public

In this case we should continue to investigate the problem through the Service Request system.

Pascal

0 项奖励
回复

5,577 次查看
JAllen
Contributor I

There is no file named MCUinit.c.o in the ObjectCode folder.  Is it created by Codewarrior?

0 项奖励
回复

5,577 次查看
JAllen
Contributor I

Codewarrior 6.3 error messages:

L1827: Symbol _vect has different size in MCUinit.c.o (2 bytes) and Vectors.c.o (46 bytes)

Link Error   : L1818: Symbol 16 - _vect duplicated in MCUinit.c.o and Vectors.c.o

Link Error   : L1301: Cannot open file C:\Documents and Settings\Dad\My Documents\Freescale Pograms etc\TWRLL64\TWRLL64_Software_Examples\TWRLL64_Quick_Start\PE_LL64_Quick_Start_Data\60_sec\ObjectCode\MCUinit.c.o

Link Error   : Link failed

0 项奖励
回复

5,577 次查看
JAllen
Contributor I

Thanks for responding.

1. Installed  CW for MCU V6.3 and updates.Pictures1-30-14 023.jpg

2. What is the Windows OS ?  Windows XP sp3.

3. What is the interface ?  Sample Micro USB.     

4. Reinstalled the device drivers from the PEMicro website.

5. See screen shot of Device Manager above.

6. See PEMicro driver test below.

Pictures1-30-14 025.jpg

0 项奖励
回复

5,577 次查看
JAllen
Contributor I

I replaced the usb cable and still no connection.

Info from Debugger command window:

executing C_layout.hwl

!OPEN source 0 0 60 39

NO CONNECTION

!Source < attributes TOOLTIP on,TOOLTIP_FORMAT signed,TOOLTIP_MODE details,FREEZE off,MARKS off

!OPEN assembly 60 0 40 31

!Assembly < attributes ADR on,CODE off,ABSADR on,SYMB off,FORMAT Auto,FREEZE off,TOPPC 0x200

!OPEN procedure 0 39 60 17

!Procedure < attributes VALUES on,TYPES off

!OPEN register 60 31 40 25

!Register < attributes FORMAT AUTO,COMPLEMENT None

!OPEN memory 60 56 40 22

!Memory < attributes FORMAT hex,COMPLEMENT None,WORD 1,ASC on,ADR on,MODE automatic,UPDATERATE 10,SHOW_ADDRESSSPACE 0,ADDRESS 0x80

!OPEN data 0 56 60 22

!Data:1 < attributes SCOPE global,COMPLEMENT None,FORMAT Symb,MODE automatic,SORT NotSort,UPDATERATE 10,NAMEWIDTH 16

!OPEN data 0 78 60 22

!Data:2 < attributes SCOPE local,COMPLEMENT None,FORMAT Symb,MODE automatic,SORT NotSort,UPDATERATE 10,NAMEWIDTH 16

!OPEN command 60 78 40 22

!Command < attributes CACHESIZE 1000

!OPEN Mcuregisters 15 38 45 41

!MCURegisters < attributes COLUMNWIDTH 0, 150,COLUMNWIDTH 1, 100,COLUMNWIDTH 2, 350,FORMAT HEX,UPDATERATE 10,MODE automatic

!bckcolor 50331647

!font 'Courier New' 9 BLACK

!AUTOSIZE on

!ACTIVATE "Data:2" "Command" "Procedure" "Data:1" "Register" "Assembly" "Memory" "Source" "MCURegisters"

done C_layout.hwl

Loading Target ...

NO CONNECTION. CHECK CABLE.

IO registers loaded for MC9S08LL64 from C:\Program Files\Freescale\CodeWarrior for Microcontrollers V6.2\prog\REG\MCU106C.REG

executing .\cmd\HCS08_FSL_OpenSourceBDM_startup.cmd

NO CONNECTION. CHECK CABLE.

!// At startup the commands written below will be executed

Target Ready

done .\cmd\HCS08_FSL_OpenSourceBDM_startup.cmd

Startup command file correctly executed.

Error: The debugger is currently not able to run

due to loss of contact with hardware.

in>

Thanks,

John Allen

0 项奖励
回复