QCVS DDR margin tool

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

QCVS DDR margin tool

13,930 Views
OneNote
Contributor I

Hi

In our latest codewarriro QCVS, the margin page of DDR validation doesn't have Margin stage as scenarios, only has Diags margin stage. Why this happen? What's the cause?

Thanks.

 

0 Kudos
Reply
22 Replies

12,950 Views
yipingwang
NXP TechSupport
NXP TechSupport

What processor are you using now?

Which version QCVS tool are you using?

0 Kudos
Reply

12,948 Views
OneNote-0
Contributor I

Thanks, Yiping.

Processor: LX2160A

QCVS version: 4.23

0 Kudos
Reply

12,946 Views
yipingwang
NXP TechSupport
NXP TechSupport

Margin stage is removed since QCVS 4.23 2020.11 release.

Margin stage scenario is no longer available for LX2, but is should be available for the rest of devices.

If further information is needed, please feel free to let me know.

0 Kudos
Reply

12,943 Views
OneNote-0
Contributor I

Thanks.

Further question: how to test margin? use diag margin stage?

 

0 Kudos
Reply

12,938 Views
yipingwang
NXP TechSupport
NXP TechSupport

I just got confirmation from the development team.

Yes, you should use the diag margin stage.

 

0 Kudos
Reply

12,828 Views
OneNote
Contributor I

Thanks.

Now it's back to 4.22.

There is a new issue happen when run the margin test.

Log attached.

read margin test log.JPG

0 Kudos
Reply

12,823 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please open CCS console on the right bottom of your task bar, type "log v", then connect to the target board again, the low level CCS log will be printed out.

Please send the CCS console log to me to do more investigation.

0 Kudos
Reply

12,818 Views
OneNote
Contributor I

ccs.JPG

 

Is this what you want? Thanks.

0 Kudos
Reply

12,816 Views
OneNote
Contributor I

CCS1.JPG

0 Kudos
Reply

12,792 Views
yipingwang
NXP TechSupport
NXP TechSupport

It failed at "reset_to_debug". If the RCW is valid, probably there is hardware design problem of the JTAG interface on your custom board.

0 Kudos
Reply

12,782 Views
OneNote
Contributor I

Measured the reset signals, when nRESET is low, PORESET_B also is low. And also found the HRESET_B is low and keep low always.Is it a clue?

0 Kudos
Reply

12,770 Views
yipingwang
NXP TechSupport
NXP TechSupport

Would you please refer to "3.2 Working with bareboard application" in the attached document to create a board board project and run it on your target board.

Please click "Target Connections->LX2160A_RDB(1)->Edit->Target Initialization File", 

please modify "USE_SAFE_RCW = False" to "USE_SAFE_RCW = True".

Then connect to the target board, and send CCS console log to me, I just want to check whether the core can be stopped.

0 Kudos
Reply

12,760 Views
OneNote
Contributor I

Print3.JPG

0 Kudos
Reply

12,758 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please modify "USE_SAFE_RCW = False" to "USE_SAFE_RCW = True" in CW initialization file and save the configuration.

0 Kudos
Reply

12,768 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please also try the following commands in CCS console.

delete all

config cc cwtap:<ip>

ccs::config_chain {lx2160a dap}

display ::ccs::get_config_chain

::ccs::stop_multi_core {21}

::ccs::reset_to_debug

0 Kudos
Reply

12,764 Views
OneNote
Contributor I

Print1.JPGPrint0.JPG

0 Kudos
Reply

12,762 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please try to run a bareboard application with hard-coded RCW as I mentioned in my previous post.

0 Kudos
Reply

12,757 Views
OneNote
Contributor I

Print4.JPG

0 Kudos
Reply

12,751 Views
yipingwang
NXP TechSupport
NXP TechSupport

As I mentioned previously, please modify "USE_SAFE_RCW = False" to "USE_SAFE_RCW = True" in CW initialization file and save the configuration, then run the bareboard application.

0 Kudos
Reply

12,786 Views
yipingwang
NXP TechSupport
NXP TechSupport

Is it possible to provide your JTAG design schematics for the custom board?

0 Kudos
Reply