Port MC1322x project (IAR) to KW2 (Codewarrior) - Seeking advice / assistance

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Port MC1322x project (IAR) to KW2 (Codewarrior) - Seeking advice / assistance

1,734 Views
rafaelsend
Contributor I

Hi,

We are attempting to migrate an embedded project that was written for the MC1322X using SMAC and RTOS in IAR to the new KW2 platform using Codewarrior. I'm not much of a coder, but the task has fallen to me at least initially and I don't have enough experience to make proper progress on it.

 

I have achieved running the SMAC Connectivity Demo on top of FreeRTOS on the KW2 in Codewarrior, so now it seems it's "just" a matter of porting the IAR application or so my manager says. However, since the new version is using Processor Expert, I'm not sure where the abstraction level needs to end and how much of the old code needs replacing as opposed to adapting.

 

If anyone has any tips as to the best way of approaching this kind of port, I would appreciate pointers or advice.

Sincerely,

 

Rafael Send

Labels (1)
0 Kudos
Reply
1 Reply

1,529 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Rafael,

CW MCU 10 does not support the Kinetis W family. This a RF family that includes software development and BU has done all work using IAR.

So can you please contact http://www.iar.com/ .

=====================================================

this answer is for you. if it helps, please click on "correct answer " button. thanks!

Best Regards,

Jennie

0 Kudos
Reply