NPF file adds S12ZVLA128 MCU

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NPF file adds S12ZVLA128 MCU

1,468 Views
leimengfighting
Contributor I

   Why CodeWarrior version 10.6 NPF file creation interface, MCU options without S12ZVLA128,How to add S12ZVLA128 chip to MCU?

-Attached is a screenshot of the MCU options.

Can someone help me,thank you very much.

.

0 Kudos
Reply
1 Reply

1,383 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Jackie lei ,

Which LIN stack do you install ? I use the v4.5.9 , it shows MC9S12ZVL128

pastedImage_1.png

Download from below link,

S12ZVM Evaluation Board|NXP   

pastedImage_5.png

Hope it helps,


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply