MQX for MK22

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MQX for MK22

1,862件の閲覧回数
myke_predko
Senior Contributor III

Hiya,

I'm migrating my product (Jade Robot - https://www.mimetics.ca) from the MK20 to the MK22 and, to simplify the move, I am going to stick with the current MQX code with a plan to port the code to FreeRTOS in the future.  

Does anybody have the MQX (10.x) initialization/characterization files for the MK22.  

Thanx!

myke

タグ(3)
0 件の賞賛
返信
2 返答(返信)

1,768件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi Myke:

MCUXpresso SDK can support MK22 with FreeRTOS. You can download SDK from below link

https://mcuxpresso.nxp.com/en/select 

For MQX, now current version is MQX v5, it is under commercial license. Please check below link for more details

MQX™ v5 Software Solutions | NXP 

MQX v4.2 is the last release in MQX classic product line.  MK22 is supported. You can create a case to  contact NXP.

https://nxpcommunity.force.com/community/ 

Regards

Daniel

0 件の賞賛
返信

1,768件の閲覧回数
myke_predko
Senior Contributor III

Hi Daniel,

Thank you for the reply.  

Sorry, I'm running MQX 4.1 (CW is version 10.4 and that's where I got that value).  

Thank you for the pointer, I'll put in the case request.

myke

0 件の賞賛
返信