MPC8641D did not halt

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC8641D did not halt

1,643件の閲覧回数
ashishkhetan
Contributor II

Hi,

I am trying evaluate MPC8641D based custom design board using Codewarrior and facing a strange problem. The boundary scan using ccs server shows the IDCODE, but when we tried to connect using debug->connect its saying "core did not halted". Did any body faced the similar kind of issue? Any points will be really helpful.

 

 

Thanks in Advanced...

@$hi$h

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 返信

1,538件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Ashish Khetan,


Most probably there is hardware design problem on your target board, please refer to the following checklist.


Ensure HRESET not tied to TRST.


HRESET to the processor exclusive to COP/JTAG header.

problems arise when the core is reset and the debugger doesn’t know about it. Usually the debugger will report the processor cannot be put into STOP mode.


Processor must be running properly in valid clocks and valid Reset clocks.

TDI/TDO/TCK tied directly to processor.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信