MPC5606S: Getting flash ID failed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5606S: Getting flash ID failed

2,904 Views
eddiewu
Contributor I

Consle Informatoion:

fl::target -lc "LC for Simple Flash"
fl::target -b 0x40000000 0xc000
fl::target -v off -l off
cmdwin::fl::device -d "MPC5606S_CODE_FLASH_VLE" -o "1Mx32x1" -a 0x0 0xfffff
cmdwin::fl::erase all
 Beginning Operation ...   
-------------------------
Chip erase not supported. Erasing sector by sector.  
Performing target initialization ...   
Reading SSCM.STATUS ...
MCU in single chip mode
Set interrupt vector base address at 0x40000000
init ECC SRAM 0x40000000:0xC000
Get application entry point ...
Searching for boot sectors ...
Found boot sector at 0x0000 and entry point at 0x220.
 Downloading Flash Device Driver ...  
 Reading flash ID .......
Error:  The algorithm was not able to run on the target or the flash is not configured properly.
Error:  Getting flash ID failed
An invalid preference was passed to the GDI protocol plugin(EPPC GDI Protocol Adapter)
Error: The algorithm was not able to run on the target or the flash is not configured properly.

Can you help me to find the error reason?

0 Kudos
Reply
3 Replies

2,782 Views
martin_kovar
NXP Employee
NXP Employee

Hello,

could you please specify, which debug probe you use and which IDE and version you use?

Regards,

Martin

0 Kudos
Reply

2,782 Views
eddiewu
Contributor I

Hi Martin, 

Sorry for late reply, I use PE Micro Multilink and Code warrior 10.7 IDE.

0 Kudos
Reply

2,782 Views
martin_kovar
NXP Employee
NXP Employee

Hello,

I am not able to reproduce this problem on my side. Could you please clarify points below?

Do you use NXP evaluation board or your own design board?

Have you ever been able to download any code into the microcontroller?

Could you please share your debug settings?

Are you sure that power supply is correct?

Regards,

Martin

0 Kudos
Reply