LittleFS Integration Support on Kinetis K70 with CodeWarrior

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LittleFS Integration Support on Kinetis K70 with CodeWarrior

1,002 Views
Tholkapiyan
Contributor I

Dear Sir,

We are working on a project using the Kinetis MK70FN1M0VMJ12 MCU with CodeWarrior IDE, and we are planning to use RAW NAND Flash for data storage.

We would like to integrate the LittleFS File System for Kinetis MK70FN1M0VMJ12 data storage Application.

Our aim is to integrate LittleFS due to its suitability for RAW NAND flash .

 While we see that LittleFS is supported in newer SDKs like that for the LPCXpresso54S018 / RW612 MCU in MCUXpresso, we need your assistance to port and integrate LittleFS with the K70 platform in Code Warrior.

Kindly provide guidance / Documentation / Application Notes / Example code for Porting Little FS to MK70FN1M0VMJ12 in code warrior.

You may also help us to suggest equivalent Filesystem to LittleFS for RAW NAND Flash - data storage ( Except FAT Filesystem ).

Thanks & Regards

V.Tholkapiyan.

0 Kudos
Reply
1 Reply

987 Views
Celeste_Liu
NXP Employee
NXP Employee

Hello @Tholkapiyan ,

Thanks for your post. For K70, we don't have such examples or application notes for integrating LittleFS into CodeWarrior. Sorry for the inconvenience caused.

You can refer to Littlefs LPCXpresso55S16 - NXP Community and the blog of Erich Styger mentioned in it. LittleFS File System with MCU Internal FLASH Memory | MCU on Eclipse

I believe they will be very helpful.

In addition, you can also consider the YAFFS Filesystem, which is also suitable for RAW NAND flash. I have found the following link for your reference:

How to port yaffs2 for MQX - NXP Community

Hope it can help you.

BRs,

Celeste

 

--------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!
--------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply