Is there a way to convert from Keil or IAR projects to CodeWarrior?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is there a way to convert from Keil or IAR projects to CodeWarrior?

2,804件の閲覧回数
rParker
Contributor I

I have purchased a license to use the CodeWarrior Tools for developing with Freescale products. Recently I purchased a TWR-WiFi-GS1500M to develop a new product but the software examples are provided for the IAR compiler only. Is there an easy way to convert the IAR project over so that I can build the project with the CodeWarrior tools that I have, otherwise the usefulness of these 'development' boards are limited.

 

I have noticed that other products offer solutions for the Keil compiler. I do not want to have to purchase all three compilers just so that I can evaluate a solution with different peripherals. I would have assumed that the Freescale supplied development boards would have been supplied with software that is supported by the Freescale CodeWarrior.

 

Thanks for any help in this matter

 

Richard.

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 返信

1,686件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

I am afraid CW doesn't  have a importer to port the IAR or Keil project to CW directly. users have to create a CW project with wizard then port the code from IAR or Keil part by part.

0 件の賞賛
返信