I wrote a program about GPIO used codewarrior10.6 for MC56F84789. When I download the program,i can't download other program for MC56F84789.but MC56F84789 is runing.,  I wrote a program about GPIO used codewarrior10.6 for MC56F84789. When I download the

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I wrote a program about GPIO used codewarrior10.6 for MC56F84789. When I download the program,i can't download other program for MC56F84789.but MC56F84789 is runing.,  I wrote a program about GPIO used codewarrior10.6 for MC56F84789. When I download the

1,061 Views
xinzhujiang
Contributor I

when i download other program ti's ok.but when i download the GPIO's program,i can't download other program.

Labels (1)
0 Kudos
Reply
1 Reply

977 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

MC56F84789 uses jtag  for on chip emulation and download.

while for MC56F84789, some jtag pin is multiplexed with GPIO. see datasheet, page 17,18.

http://www.nxp.com/files/dsp/doc/data_sheet/MC56F844XX.pdf?fasp=1&WT_TYPE=Data%20Sheets&WT_VENDOR=FR... 

if you defile the related jtag pin as GPIO, the jtag feature can not work  normal.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply