I'd like to inquire about the codewarrior.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I'd like to inquire about the codewarrior.

1,824 Views
Leekiho
Contributor I

I'm going to read firmware with Multilink tool for NXP-based ICMP56-based IC.

​

I'm going to save the data stored in the IC and upload it again.

​

The program is Codewarrior. I want to save it as a Hex or ef file and upload it again, so please tell me how.

0 Kudos
Reply
3 Replies

1,757 Views
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @Leekiho,

Do you need to create a hex/elf file for flashing the device? If so, you can set "Create Flash Image" to generate an image file.

Julin_AragnM_0-1721255244498.png

You can also take a look into these posts:

Best regards,
Julián

0 Kudos
Reply

1,801 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hello Leekiho,

You mentioned "INXP-based ICMP56-based IC". Could you please be more specific about the part number? This information is important to find the right IDE version.

Thanks,

Jun Zhang

 

0 Kudos
Reply

1,781 Views
Leekiho
Contributor I
I'm sorry. I think I misrepresented it It is an IC component, MPC5604.
0 Kudos
Reply