I am trying to update the software in a MC9S12DP512 using a PE Micro Multilink Universal.  Some old instrustions I have use “Codewarrior for HC12 V4.6” and the “hiwave.exe” command.  I’m evaluating CodeWarrior® Development Studio for HCS12(X) Microcontrol

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I am trying to update the software in a MC9S12DP512 using a PE Micro Multilink Universal.  Some old instrustions I have use “Codewarrior for HC12 V4.6” and the “hiwave.exe” command.  I’m evaluating CodeWarrior® Development Studio for HCS12(X) Microcontrol

675件の閲覧回数
neilurbahn
Contributor I

I am trying to update the software in a MC9S12DP512 using a PE Micro Multilink Universal. Some old instrustions I have use “Codewarrior for HC12 V4.6” and the “hiwave.exe” command.

I’m evaluating CodeWarrior® Development Studio for HCS12(X) Microcontrollers (Classic IDE) v5.2. It seems OK, but it does not have option for MC9S12DP512.

Is that only available with the licensed version and an update?

ラベル(1)
0 件の賞賛
返信
1 返信

638件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

hi

please refer answer in this thread

https://community.nxp.com/thread/434029 


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信