How to patch the codewarriorIDE without updater

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to patch the codewarriorIDE without updater

3,198 Views
johnnywang
Contributor I

I con't updata the software with the updater,is there a way to patch the IDE with the download files?And patch the Service Pack with the download files?How to do it?

Thank you!

0 Kudos
Reply
3 Replies

3,087 Views
johnnywang
Contributor I

CodeWarrior for PA (windows) V8.8, patch file:CW PA v8.8.x for P2020 Windows Update,CW PA v8.8.3 Application Edition - Patch.

0 Kudos
Reply

3,087 Views
Alexis_A
NXP TechSupport
NXP TechSupport

Hello Johnny,

Inside the CW PA v8.8.x for P2020 Windows Update there's the instructions for install this software package:

=======================================================
Installation Instructions
=======================================================
1) Install CodeWarrior Development Studio for Power 
Architecture Professional Edition Release v8.8 Golden 
Master (build 80229) 

2) Install the 8.8.3 patch over this (build 90619) 

3) Install the already released P2020 Service Pack 1 
1070 (Windows) / 1080 (Linux) 

4) Extract the Service Pack Update archive on top of 
the 8.8 release with the 8.8.3 patch and with P2020 
Service Pack 1 ‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍

Best Regards,

Alexis Andalon

0 Kudos
Reply

3,087 Views
Alexis_A
NXP TechSupport
NXP TechSupport

Hello johnnywang‌,

Can you let me know which code warrior version and patches are you trying to install?

Best Regards,

Alexis Andalon

0 Kudos
Reply