How to Create & Use Library

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to Create & Use Library

2,280 Views
mayursavaj
Contributor III

Hi Everyone,

 

I want to create Library and want to use in other project.

My question is like.. How to create Library files and use to other project without sharing my Code?

 

I am using Code Warrior 10.6

 

 

 

Thanks in advance,

Mayur Savaj

Labels (1)
0 Kudos
Reply
3 Replies

2,083 Views
BlackNight
NXP Employee
NXP Employee

Hi Mayur,

I believe the following article should answer your question: Creating and using Libraries with ARM gcc and Eclipse | MCU on Eclipse 

I hope this helps,

Erich

0 Kudos
Reply

2,083 Views
mayursavaj
Contributor III

Hi Erich,

Library is created. But unable to use that library files to Other project. (I am getting "invalid variable"  as error).

I m using CW 10.6

Thanks,

Mayur

0 Kudos
Reply

2,083 Views
BlackNight
NXP Employee
NXP Employee

Hi Mayur,

I'm not sure if I can follow? Can you post a screenshot?

Erich

0 Kudos
Reply